You are here: Preface > Learning Kollmorgen Automation Suite > Read KAS Manuals

Read KAS Manuals

If you prefer to read printed material, the following manuals (in PDF format) are available:

KAS Title PDF Description
Release Notes The KAS version 2.11 Release Notes contain fixed limitations, known limitations, workarounds, and information on all hardware and software components that have been updated, changed or added in this release.
Getting Started

Covers the main steps to get your KAS system up and running

30 Minutes to Motion

Covers the main topics to help you start quickly with KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger. The objective is to familiarize you with the basic principles and the way the program works by creating a simple motion application project.

IDE User Manual Contains the content to help you with KAS IDE, except the topics included in the Reference Manuals
Reference Manual - PLC Library Contains Technical References on PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Programming Languages and Library
Reference Manual - Motion Library Contains Technical References on Motion Library for Pipe Network and PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML
KAS PAC"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system Webserver User Manual This document provides information on how to access, use and maintain the PAC webserver.
KAS PDMM/PCMM Webserver User Manual This document provides information on how to access, use and maintain the PDMM or PCMM webserver.

Table 1-2: List of KAS Guides in PDF Format

See also the full list of deliverables here

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™